Issue
Xenta Server Error: "Sequences number in unit was reset. Fetching from first event."
Environment
- Xenta Server
- Xenta 511, 511:B, 527, 701, 711, 721 and 731
- Xenta Error Log
Cause
When Vista asks the Xenta Server for log data,it is returned unexpected data
Resolution
Reinstalling or upgrading to a System Program version >5.14 SP1 should correct this issue.