Issue
Need to add new generation of Infinet controller(s) to existing NetController with old system such as Infinity system with SX8000 and Continuum 1.4 or older version.
Environment
Continuum , SX8000
Net Controller / NetController (CX9900 , CX9940 , CX9000 , CX9200 , CX9400 , CX9702 )
Infinet controller (i2 controller , i1 controller)
Cause
Older version of Continuum (v1.4 and older) and Infinity system (SX8000) does not provide controller type of i2 controller when you create Infinet controller under NetController.
Resolution
The i2 controller (including i286x–V models) can be used as direct replacements for existing Continuum VAV controllers on all versions of Continuum and SX8000 installations. Select the controller type of the same model number.
I.e. : For i2865-V , select TCX865 .