Using i2 controllers with a CMX241

Issue

Will an i2 device work on an existing installation that uses a CMX241 controller?

Product Line

Andover Continuum

Environment

Continuum

CMX241

Infinet

Cause

An installation that has a CMX controller with infinet and the infinet 1 controller needs to be replaced with an i2.

Resolution

The CMX241 controller will recognize an i2 controller, but it will handle it as if it is an infinet1 controller.

Some infinity system variables and their functionality will not be recognized such as accrestart mode, accstatusflash, etc...

The replacement for the CMX241 is the BCX9640