Issue
There are several workstations in a LAN network. Some workstations can display correctly in the Continuum explorer object tree, but some workstations can not. All of the workstations can display in the listview. All the devices can do teach correctly.
Environment
- Windows XP Sp3
- Continuum 1.92
Cause
The outofservice check box has been checked
Resolution
- From the listview, select the workstation which can't display correctly
- Right click on the workstation and select open
- From the general page, uncheck outofservice
- Restart Continuum.