Issue
When editing a personnel object an error is received "Input string was not in a correct format" using 1.82 or 1.90.
Product Line
Andover Continuum
Environment
Webclient
Windows XP
Windows Vista
Windows 7
Windows Server 2003
Windows Server 2008
Cause
Microsoft released .Net 2.0 SP2 which caused an issue with our code in the personnel area.
Resolution
The version of Continuum you are using will determine the solution you need to use.
1.82 - Uninstall .net 2.0 SP2
1.90- Install the following hotfix
The issue was corrected in 1.91.