Issue
As part of installing InVue, what are the licensing requirements?
Environment
InVue 1.1
Cause
InVue software re-installation on new server hardware.
Resolution
Two license files are required. One license is for the Wonderware core and one license is for the add-on programs (like TreeTech, interface drivers, hrdbdde driver, etc...).
The Wonderware license file was typically provided on a 3.5" floppy diskette.
The filename is wwsuite.lic.
It is installed in the following path: C:\Program Files\FactorySuite\Common\License
Install the file by using Wonderware's License Utility (available via Start > Programs > Wonderware FactorySuite > Common > License Utility).
The license file for the add-on programs is provided during the software installation process. Unlock codes must be provided to allow the programs to run. A 30-day temporary license is provided during installation.
The filename is WIBSSuite.lic.
It is installed in the following path: C:\Program Files\Siebe\WIBs\Core
When the unlock codes are provided, use the Purchase WIB Software shortcut (placed on the desktop during software installation) to enter them.