Issue
Self-Registration Error while installing Remote Workstation (some of the "dll" files are not installed). The following files did not self-register or unregister.
Environment
TAC Vista 5.0.X
Remote Workstation
Cause
When uninstalling the TAC Vista Remote Workstation some of the "dll" files will not un-install from "TAC Shared" folder (Find the TAC Shared folder in "C:\Program Files\Common Files).
Due to this, while reinstalling the Remote Workstation pop-up an error-"Self-Registration" and few "dll" cannot install, then the Installation terminates.
Resolution
- Uninstall the Remote Workstation.
-
Delete the TAC Shared folder from C:\Program Files\Common Files
- Reinstall Remote Workstation.
Note: Install .NET Framework 2.0 before installing the Remote Workstation software.