Issue
Is it recommended to modify TGML Graphics from Remote Workstation?
Product Line
TAC Vista
Environment
TAC Remote Workstation
TAC Graphics Editor
Cause
Remote Workstation should not be used as an engineering tool. It is used only to access the system.
Resolution
Remote Workstation's recommended use is to access the system. Its function is not meant to be used as an engineering tool.
It is possible to access the TGML Graphic pages from remote workstation to monitor and modify the objects not for editing Graphic Pages.
You can prevent the access for TGML Graphics from Remote Workstation. For settings, please refer to Lessons Learned Article Lessons Learned Article #4901.