Issue
When exporting a pointslist from VisiSat 2.1 build 148 to XBuilder (See pdf link in Resolution below), the format of the TACXBuilder.xmlm is not aligned in a manner that XBuilder fully understands.
Environment
- Xenta
- VisiSat
- Points list
- Export
Cause
TACXBuilder.xmlm is not aligned in a manner that XBuilder fully understands.
Resolution
Install service pack 1 for VisiSat 2.1 build 148.
For further information see TPA-LOND-08-0006.00
The Service pack for VisiSat 2.1 build 148 can be downloaded here.
The current version of VisiSat is version 2.1 build 201 (September 2018)
VisiSat 2.1 Build 196 can be download here.
Two service packs are available: -
for information and a download link for service pack 1 software click here.
for information and a download link for service pack 2 software click here.