Issue
A Network 8000 LCM-84x10 or LCM-88x10 will be integrated with a Niagara R2 UNC. What firmware revision level must the LCM have for proper operation?
Environment
Network 8000 LCM
Niagara R2 UNC-520
Cause
The integration requires the LCM to have at least Year 2000 firmware installed. The shadow objects in the Niagara station will not update or function properly.
Resolution
Upgrade the LCM using EPROM kit # LCMA-138-54.
This kit is to be used with the LCM-84x10 or LCM-88x10 and it will upgrade the firmware level to 5.4, Year 2000 compliancy.
It is available for purchase via iPortal.