BAS 2800+ - Adding a Short Form Edit command to a User Menu.

Issue

Adding a "Short Form Edit" command to a User Menu.

Product Line

Other

Environment

  • BAS 2800+
  • BAS2800+
  • Short Form Edit
  • User Menus

Cause

This option is not available by default.

Resolution

  1. The add this option select "System Setup / User Menus"
  2. Select to create a "New Command"
  3. Complete command details as shown below.
  4. Having created this command add it to the required menus.