Issue
How are devices added or removed from the monitored list?
Environment
Sigma
4.05
4.05 SEB
Device Monitor
Adding
Removing
Cause
Confusion over how devices are added or removed.
Resolution
To add devices to, or remove devices from, the monitored list is achieved as follows:
Enter Sigma "System Setup" and select "Networks and Devices".
Select the "Zone Name" and choose the "Device Monitor" tab.
The screen shot below shows the devices being monitored, this list is formed from the DeviceCNF.rec file.
To prevent a device from being polled, tick the appropriate "Omit" box.
To add devices select the "Add" button, complete the device name and IP address.