Issue
A mothballed government building is being put back into use. It uses a DMS-35 with some Microsmart controllers for building automation and control. What does the DMS-35 look like and what are its dimensions? The customer wants to install power and communications to it. The connectors for these cables are missing. What do they look like?
Environment
DMS-35
Cause
n/a
Resolution
Digital photos of a DMS-35 are provided.
Scanned images of the obsolete installation guideline (portions thereof) are provided.