Issue
A particular turnstile requires a one second pulse, thus the door is configured with a one second strike time, turnstile works fine but getting intermittent forced entry alarms when person takes more than a second to go thru.
Environment
CyberStation
ACX5740
ACX5720
CX9680
CX9900
AC1
AC1Plus
Cause
Continuum generates forced entry if door switch opens after the door strike time has expired.
Resolution
In the door editor, go to the 'Channels' tab and enter a value for ForcedEntryDelay.
For example:
Entering a value of 3 suppresses door forced enter for 3 seconds following valid access (or Request to exit) at the door.