Upgrading Vista system with TAC Danduc OPC server

Issue

Does TAC Vista 5.1.6 work with a TAC Danduc OPC server?

What OS works with TAC Danduc OPC server? 

Product Line

TAC Vista

Environment

TAC Vista 5.1.6

Cause

TAC Danduc OPC server is tested on many sites in Denmark using Vista 5.1.6.

Only 32-bit OS works with TAC Danduc OPC server.

Resolution

TAC Vista 5.1.6 is works fine with TAC Danduc OPC server.

All operating systems also work fine as long as they are 32-bit.