Xenta Controllers are 1 hour ahead of PC time.

Issue

Xenta controllers are 1 hour ahead of PC  time.

All controllers and PC are in the same timezone and have the same daylight offset time.

Product Line

TAC Vista

Environment

Windows XP Service Pack 1 and 2

Cause

Windows daylight times are incorrect for the current dates.

The PC time is in normal time not Daylight time even though the update daylight saving automatically is selected.

Resolution

Install windows update KB955839. This updates the daylight dates in windows.

Click here to download this update