Issue
Error javax.baja.sys.NoSuchSlotException: textOverride when activating KitPx "Export' button for pdf in G3 version 3.6.
Environment
I/A Series G3 (version 3.6)
Cause
KitPx 'Export' button included on a canvas as part of a ReportPx. Activating the 'Export' button causes the export to pdf to fail with the following exception ... javax.baja.sys.NoSuchSlotException: textOverride.
Resolution
Upgrade the pdf module to 3.6.38 or higher. The zip file (pdf-3.6.38.zip) can be downloaded from The Exchange Download Center.