Issue
An Alarm object in an XBuilder project has two outputs - digital and state. The state output corresponds to the acknowledged state of the alarm. To use this output programmatically, the enumeration values must be known.
Environment
Xenta 511,527,555,701,711,721,731
Cause
Not knowing meaning of Alarm State output values in Xenta 700
Resolution
The Xenta 700 alarm state enumeration is:
0 - Normal
1 - Passive_unacked
2 - Active_unacked
3 - Active_acked