Issue
Can the Anti-Passback rules be ignored for certain personnel cards?
Environment
Access Control:
CX9702
CX9900 with AC1 modules
CX9680 Netcontroller II with AC1 Modules
ACX5720, ACX5740
Cause
Often certain site personnel require free access around a site e.g. Security personnel or management.
Resolution
If Area Anti-Passback is being used then there is the “AllowEntEntEgr” attribute in the personnel object, it is named “Allow Passback Entry” in the Personnel Manager. This attribute is by default False, but can be set to True in any Personnel to ignore Area Anti-Passback rules.
This attribute does not apply to Timed Anti-Passback.