How to Node a BAS outstation. What are the node commands?

Issue

How to Node a BAS outstation.

What are the node commands.

Product Line

Other

Environment

BAS

UNC532

UNC496

UNC596

Cause

What are the node commands.

Resolution

Using either the pocket terminal utility or using hyper terminal, plug in the lead into SK1, the terminal will go "ready"

Using the commands as follows:

Note1: "O" is as in letter O.

Note2: "H132" does not apply to a x96 controller.

Note3: "S" displays the current node setup.