Issue
Need to save the application, configuration and COV link data for an MNB-controller so that in the event the controller fails, all the information can be easily reloaded into a new controller.
Environment
MNB family controllers
WorkPlace Commissioning Tool, version 5.7.2 or newer
Cause
Need to save the application, configuration and COV link data for an MNB-controller so that in the event the controller fails, all the information can be easily reloaded into a new controller.
Resolution
The Backup and Restore facility of WorkPlace Commissioning Tool allows the user to backup the complete controller application, configuration, flow balance and COV link data for a single or multiple controllers or restore of a single controller on a given network in a simple operation. The procedures for using the Backup and Restore functions of the WPCT are included in the WorkPlace Tech Tool version 5.7.2 release notes. The Backup and Restore documentation is available via this WorkPlace Tech Tool release 5.7.3 Release Notes from The Exchange Download Center.