Veeder Root Xdrivers

Issue

Are the current Veeder Root Xdrivers compatible with the TLS450 and TLS2P console?

Product Line

Andover Continuum

Environment

Xdriver

Cause

The current Xdrivers are compatible with the Veeder-Root TLS350 Console. Are the current Veeder-Root Xdrivers compatible with the TLS450 and TLS2P console?

Resolution

No. The current 1st and 2nd Generation Continuum compatible xDriver for Veeder-Root TSL300/350/350R is not compatible with the TLS450 or TLS2P. For the current Xdriver see
Leak Detection Systems Drivers on The Exchange  Download Center.