Old Generation Temperature Sensors, New Generation Temperature Sensors, CXR, CXT, CZT, CSC5252, CSC5352.

Issue

Can old generation temperature sensors or new generation temperature sensors be used on CXR, CXT, CZT, CSC5252, CSC5352 ?

Product Line

Field Devices

Environment

CXR

CXT

CZT

CSC

CSC5252

CSC5352

CSC 5252

CSC 5352

Cause

Can old generation sensors or new generation sensors be used on CXR, CXT, CZT, CSC5252, CSC5352?

Resolution

Existing old generation sensors can be used on the current range of discrete controller, however they CANNOT be used/mixed with new generation sensors.

Note, when replacing sensors or upgrading a controller to the current version, terminal numbers are different between old generation and new generation sensors, see the datasheet for terminal numbers.

For the CXT datasheet click here.

For the CXR datasheet click here.

For the CZT datasheet click here.

For the CSC5252 or 5352 datasheet click here.