Multiple Monitors on I/NET

Issue

Drop downs not visible on secondary monitor used with I/NET

Product Line

TAC I/NET

Environment

Windows XP

I/NET Seven 2.41

Cause

As of 2.41 I/NET is not intended to be a multiple monitor platform

Resolution

  1. Modify the display settings to configure the monitor with the I/NET display as the primary monitor
  2. Upgrade to I/NET 2.41 using Windows 7 as this problem has not been seen with this specific installation
  3. Use I/NET on your primary monitor and AMT on your secondary monitor.

If it doesn't work, please refer to Lessons Learned Article LL#15586.