Issue
Are there any specific setting to be enabled in order for restricting
the access to TAC Vista database folders? Currently all windows users can
copy the TAC Vista database folders.
Environment
Vista 5.1.6
Cause
The only way to restrict the access to Vista database folders is to create a special Windows user which have full access to the folders and then the Vista server must run as a service logged on with this Windows user.
Resolution
Create a special Windows user which is administrator on the PC, run the service Tacos with this user.
Restrict the access to the database folders for all other Windows users.