Host Lost Message Definition

Issue

Host Lost Message Definition

Product Line

TAC I/NET

Environment

I/NET

Cause

Host Lost messages are caused when I/NET has lost communication over the Ethernet LAN with a host workstation, Xenta 527 or NPR.

Resolution

Host masks are enabled or disabled by using the far left bit mask of group 1. 

You can enable/disable these from showing up in AMT by:

  1. Open AMT
  2. Select Edit>Configuration
  3. Toggle the far left bit of Group 1
  4. Click OK

 

Alternative Resolution

  1. Open I/NET configuration
  2. Modify the Active Profile
  3. Click Host Masks
  4. Modify Each Host Device
  5. Toggle the far left bit of Group 1