Replacement of Satchwell VG combined Actuator & 2-port Valve Body assembly due to obsolescence.

Issue

Satchwell “VG” combined Actuator & 2-port Valve Body assembly requires replacement.

Product Line

Field Devices

Environment

  • Stand alone Satchwell “VG” combined Actuator & 2-port Valve Body assembly
  • VG
  • Actuator
  • 2-port
  • Valve Body

Cause

Obsolescence of Satchwell “VG” combined Actuator & 2-port Valve Body assembly.

Resolution

Replace Satchwell “VG” combined Actuator & 2-port Valve Body assembly with Schneider Electric MD10B Actuator, LMD-MB Linkage Kit and Satchwell MB series 3-port Valve Body of appropriate size.

N.B. 

The MB 3-port Valve Body may be converted to a 2-port Valve Body by installing a plug in Port 3

 

Details of the original Satchwell “VG” combined Actuator & 2-port Valve Body assembly may be viewed here.

Details of the replacement Schneider Electric MD10B Actuator may be viewed here.

Details of the replacement Schneider Electric LMD-MB Linkage Kit may be viewed here.

Details of the replacement Satchwell MB 3-port Valve Body may be viewed here.

N.B.

It is possible that the "VG" Actuator may have been fitted with an Auxiliary Switch.

If so then an MD-S1 Auxiliary Switch may be fitted to the MD10B Actuator if required.

Details of the MD-S1 Auxiliary Switch may be viewed here.