Issue
Unable to open a time chart via TGML graphic in webstation. The same graphic works in workstation.
Environment
TAC Vista 5.1.X - workstation & Webstation
TGML Editor 1.1.X
Cause
Binding to the PV value of a time chart isn't the correct way to do this, but workstation is unable to display a dialogue for an object that has multiple properties and so displays the complete time chart.
Resolution
A link should be used that is linked to the time chart object
Attached is a TGML component adapted from the standard analogue clock component that explains how to do this. The binding should be bound to -your time chart-