Veris HW sensor part number for displaying both the temperature and humidity readings on the sensor's LCD

Issue

Veris HW sensor part number for displaying both the temperature and humidity readings on the sensor's LCD

Product Line

Field Devices

Environment

Veris HW Series deluxe wall humidity sensors

Cause

There is a need to display both the humidity and temperature readings on the sensor's LCD

Resolution

In order for unit to display both temperature and humidity, use the TA or D temp selection in the part number.

Refer to the HW series sensors datasheet.