Issue
Building a database to take to a site and the doors do not show up in Netcon, though they can be controlled.
Environment
I/NET versions 2.10 and up using SCU 1284s.
Cause
The controller has not recognized the doors in the SCU and has to be readded in Netcon to be saved again.
Resolution
To resolve this there are a few simple steps that needs to be followed to get this to work again.
- Connect to the controller and then go to Edit/Host Computer/Network Configuration.
- Penetrate the Link Summary, Controller and then SCU.
- In the cnf column there should be a -- sign indicating that there is no communication to the device.
- Click on the delete button to remove it from the SCU.
- Close all the Editors and then go back to the controller.
- Go to Resident I/O Points, if the door point exists, delete it and close out of the editor.
- Open up the Resident I/O Points and re-add the point again and repeat Step 2.
- Save the doors now as Step would have a + sign indicating that there is communication to the device.