I/A Series R2 OBIX Driver part number

Issue

I/A Series R2 OBIX Driver part number

Product Line

TAC I/A Series

Environment

I/A Series R2 Enterprise Server / Universal Network Controller (UNC)

Cause

In order for an I/A Series R2 Enterprise Server or UNC to function as an OBIX server, the Enterprise Server or UNC needs to be licensed for it. This is required for integration to I/A Series G3. Refer to Lesson Learned Article #3385.

Resolution

Part number: IA-DRV-OBIX

This is the part number required for each Enterprise Server / UNC that needs to function as an OBIX server.