Issue
Need to configure more than one card format not natively supported in Continuum.
Environment
CyberStation
CX9900
CX9702
CX9680
ACX5720
ACX5740
Cause
Documentation
Resolution
Continuum controllers support up to four (4) custom cards.
Custom cards 2-4 are configured in the same way as the first custom card format, the only exception is the name of the magic InfinityNumeric.
When creating the InfinityNumeric that contains the array for the card format, use...
AccessFormat for the first custom format
AccessFormat2 for the second
AccessFormat3 for the third
AccessFormat4 for the fourth and last one supported.