Issue
I/A Series R2 graphics browsing issue when using Windows 7 64-bit computer and Internet Explorer 9
Environment
- Windows 7 (32-bit or 64-bit)
- Internet Explorer 9
Cause
Java 1.6 Update 28 compatibility issue with IE9
Resolution
Java 1.6 update 29 or later is required when using IE9