Issue
Trying to get a schedule working in a MNB-1000 and getting the following error message:
Schedule Setup Wizard will not run: Not supported for this application's type of device. Device type: 971
Environment
MNB-1000
MNL controllers
Workplace Tech
Cause
New to programming the MNB controller line
Resolution
A 7-day schedule object is available for the MNB-1000 (only) and is part of the Schedule Control stencil.
The Schedule Setup option under the Application drop-down menu only applies to MNL applications.