Issue
When swiping card, the status of door point in Controller Summary doesn't change.
Environment
I/NET
Cause
This is so designed in I/NET
Resolution
In I/NET, the status door point doesn't change when swiping card. So if interaction with swiping card is needed, you need to use Access Initial Control or create another real External point for the door point. (00/01 Ext apart from 08/09 Int)