Issue
How can the default graphic for the Monitor Screens be modified in SIGNAL?
Environment
SIGNAL (all versions)
Cause
A re-installation of SIGNAL from floppy restores a default graphic called _MAINMAP.SSF when clicking on the Monitor Screens.
Resolution
Sign onto SIGNAL with administrative privileges and click on the Edit drop-down menu. Select Edit Button.
The mouse changes to a hand with an index finger pointer. Select the Monitor button. The pop-up below will appear:
Change the filename _MAINMAP.SSF to the desired ssf file and click Save/Done.