Issue
What I/A Series G3 driver can be used to directly interface a McQuay MicroTech OPM with Microtech legacy controllers to the ENC-520?
Environment
I/A Series G3, ENC-520
Cause
The existing system includes McQuay legacy products (e.g MicroTech 1 controllers) communicating to a MicroTech OPM (Open Protocol Master) panel. The system does not support open protocols such as BACnet or LonWorks.
Resolution
The McQuay driver communicates to the MicroTech legacy devices through the McQuay OPM. The driver is compatible with I/A Series G3 versions 3.4 and higher. The part number through Schneider Electric is ENC-DRV-MCQ.
Click here to download the Niagara McQuay Driver Guide.