Field Devices - Cannot connect MD actuator to MBX valve, using appropriate linkage.

Issue

Cannot connect MD20B-230 actuator to MBX4451 valve, using a 914-1071-000 linkage.

Product Line

Field Devices

Environment

  • MD Actuator
  • MB valve
  • MBX valve
  • Linkage

Cause

The existing documentation is very unclear and shows the wrong bracket.

Resolution

The issue arises initially in that a different bracket is shown in the current documentation.

The second issue is that there is a circlip on the back of the actuator which must be positioned before fitting the bracket. Below is a picture showing the correctly circlip and bracket. Please take note of the circlip position.

Revised documentation will be available in due cause.