Restore from Local Host Grayed out.

Issue

Unable to set up Automatic DPU Restore on a local Host PC as the option is grayed out.

Product Line

TAC I/NET

Environment

I/Net version 2.XX and above.

Cause

When the system is using the Server/Remote Client application the changes can only be done from the PC or Server.

Resolution

To resolve this issue the Automatic DPU Restore needs to be enabled at the Host PC or server so that the PC that is making the changes will automatically download them to the necessary DPUs. LL article 5381 describes how this should be done.