Issue
Can we integrate 3rd party LON devices
Product Line
SmartStruxure Solution
Environment
StruxureWare Building Operation AS or Enterprise Server
Cause
Integrating third part LON devices allows the system to take full advantage of the open protocol.
Resolution
We currently support 3rd party Lon devices in Version 1.0 and 1.1, but some large devices are too big to be configured in quantities according to specifications. No major change regarding this is scheduled until earliest 1.4.
In 1.3 we will change the numbers that we support to configure but this will mainly be runtime improvements. Some devices can only be configured with Lonmaker which is an extra step during the engineering process.