Issue
Trying to install I/NET on 64-bit PCs.
Environment
- I/NET 2.40 and above
- Windows 7 64-bit
Cause
The 64-bit operating system is not currently supported in the existing versions of software.
Resolution
The next release of software scheduled for the Mid 2012, version 2.42 would be compatible with the 64-bit operating system.