Issue
When ordering a Vista Server license module, is there a Workstation license included?
Environment
TAC Vista 5.x
Cause
When ordering a Vista software Package, a Workstation license module is usually included (see licensing package matrix in related documentation), but when using a Vista server license, it does not also include a Workstation license.
Resolution
No Vista Workstation license is included in the Server license. The Workstation license modules are dealt with separately, and if several simultaneous Workstations running are required, the equal amount of Workstation licenses are required.