Is it possible to create host bindings to Vista using NL220?

Issue

Is it possible to create host bindings to Vista using NL220?

Product Line

TAC Vista

Environment

  • Vista 5.1.7
  • NL220

Cause

Yes it is possible but you must use a Loytec network interface

Resolution

Create binding to the LON interface in NL220 and use the Vista System Plug-in to import the project to Vista