Photo is blurry when capturing into CyberStation.

Issue

Using a webcam a photo is captured. When attempting to save the captured image to a personnel record it comes in blurry.

Product Line

Andover Continuum

Environment

CyberStation with Episuite Badging option

Webcam

Cause

Captured photo quality in personnel editor is poor. Captured photo in webcam software is excellent.  

Resolution

The device driver in the image source properties dialog box was changed from the webcam driver to the Windows driver.