Issue
At times there is a need to keep a door unlocked with a schedule, but this can cause a problem if there is extreme weather and no one is at the building.
Environment
- Continuum
- AC1/AC1A
- AC1 Plus
- ACX5740
- ACX781
Cause
Leaving a buildings door open when there is no one at the building is a security risk. This work around will take care of this problem.
Resolution
The way around the issue of having a door open from a schedule when no one is in the building due to inclement weather is to set up a Plain English program to set the Unlock InfinityNumeric On only if the schedule InfinityNumeric is On AND there has been a valid access to the door.
InfinityProgram
FlowType Loopin
Objects required
- Door1 - the name of the door to control
- SchedNum - InfinityNumeric controlled by the schedule
- UnlockNum - InfinityNumeric linked to Door1 Door Unlock Schedule
Code Example (This must be edited to reflect the door name and schedule numeric that has been created)
WaitForSched:
UnlockNum=Off
If SchedNum=On then GoTo WaitForValid
WaitForValid:
If Door1 ValidAccess is True then
UnlockNum=On
GoTo WaitForEnd
Endif
WaitForEnd:
If SchedNum=Off then GoTo WaitForSched