Issue
Where is the 0-10 volt control signal connected, on a Forta actuator?
Environment
Forta
M400
Actuator
Wiring
Connections
Cause
The customer was uncertain how to connect the M400 actuator.
Resolution
The general configuration and connection details are the same for all of the Forta range of actuators.
All of the range can accept a 0-10 volt dc input or increase/decrease signals.
Terminal Function Designation
G 24 V AC Supply
G0 24 V AC return
X1 Input
MX Input, neutral
VH Increase
VC Decrease
G1 16 V DC Supply for RC
Y 0–100 % Feedback signal
The 0-10 volt control signal is connected to (X1) and the associate 0 volt is connected to (MX).
If there is not an associated 0 volt available then (MX) should be connected to the (G0) terminal.
To download the Forta Handbook please click HERE.