Script programs in b3 controllers will not autostart after reboot of the controller

Issue

Script programs in b3 controllers will not autostart after reboot of the controller

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation AS-B

Cause

The program is not configured to autostart in StruxureWare Building Operation.

Resolution

In the Properties of the program object, ensure that the Restart and Autostart fields are set to True.