Issue
What Sigma documentation comes with Sigma
Product Line
Satchwell Sigma
Environment
Sigma
Cause
Is there any documentation that can be viewed other than via the "Help" menu on the Sigma Client.
Resolution
The Sigma Help file Sigmahelp.chm is located in C:\Sigma\Help.
The file can be copied to any other PC or memory stick and viewed by double clicking on it.
The help file is best viewed in IE8 or IE9 in compatibility mode.