Issue
Need to print a variable such as DayOfYear and have the value always printed using three digits.
Environment
All CXs
All i2s
All b3s
Cause
Documentation
Resolution
Use the 'Right' function as follows...
Print Right("000",DOY,3) to MyString
The above will print the day of the year to MyString padded with zeros to the left when day of year contains less than three digits.