Issue
The Platform Software Manager indicates the Report module is installed on the ENC, but ReportService cannot be added to the Services container of an ENC.
The following error message is displayed in the Program Director window:
WARNING [22:25:05 12-Jan-12 CST][sys.xml] Type "report:ReportService" not found: null [3:55]
javax.baja.xml.XException: Error parsing value [4:4]
at javax.baja.io.BogDecoder.err(BogDecoder.java)
at javax.baja.io.BogDecoder.decode(BogDecoder.java)
at javax.baja.sync.AddOp.decode(AddOp.java)
at javax.baja.sync.SyncBuffer.decode(SyncBuffer.java)
at com.tridium.fox.sys.broker.BBrokerChannel.syncToMaster(BBrokerChannel.java)
at com.tridium.fox.sys.broker.BBrokerChannel.circuitOpened(BBrokerChannel.java)
at com.tridium.fox.sys.BFoxConnection.circuitOpened(BFoxConnection.java)
at com.tridium.fox.session.SessionCircuits$ServiceThread.run(SessionCircuits.java)
at java.lang.Thread.run(Thread.java:823)
Environment
Niagara G3 all versions, ENC-410, ENC-520
Cause
The ReportService Module in the ENC Platform may have become corrupted.
Resolution
Uninstall and reinstall the module in the ENC, making sure the module content filter is set to ui+runtime.